Reset (FB)

FUNCTION_BLOCK Reset EXTENDS BaseService

This function block is used for calling the reset service of a specific instance of a CIP object. The exact effect of this service depends on the CIP object (refer to the CIP specifications (Vol. 1 and 2). This instance call resets the DEVICE_123_ETHERNET device as soon as xExecute yields TRUE:

PROGRAM PLC_PRG
VAR
    reset : ENIP.Reset ;
END_VAR

reset(
    xExecute:= ,
    itfEtherNetIPDevice:= DEVICE_123_ETHERNET,  (* instance of the device (instance is found in the I/O Mapping of the device) *)
    eClass:= ENIP.CIPClass.IdentityObject,      (* cip class which contains the desired attribute *)
    dwInstance:= 1,                             (* value of 0 is class level, range from 1..x is instance level *)
    xDone=> ,
    xBusy=> ,
    xError=> ,
    eError=> );
    ;
InOut:

Scope

Name

Type

Inherited from

Input

xExecute

BOOL

ETrig

Output

xDone

BOOL

ETrig

xBusy

BOOL

ETrig

xError

BOOL

ETrig

Input

itfEtherNetIPDevice

IEtherNetIPService

BaseService

eClass

CIPClass

BaseService

dwInstance

DWORD

BaseService

tTimeOut

TIME

BaseService

Output

eError

ERROR

BaseService