ID_TO_ADDR (FB)
FUNCTION_BLOCK ID_TO_ADDR
The function block ID_TO_ADDR converts the handle used for the Communication Function Blocks to the physical identification of a slot of a PROFIBUS DP-slave or subslot of a PROFINET IO Device.
Code-Example: see RALARM
- InOut:
Scope
Name
Type
Initial
Comment
Input
ENBOOLTRUE
Enable
IDDWORDSlot or subslot handle
Output
ENOBOOLFlag
STATUSDWORDLast detected status
Inout
ADDRPhysical address information