TCP_Processor (FB)
FUNCTION_BLOCK ABSTRACT TCP_Processor EXTENDS LConC IMPLEMENTS ITCPProcessor
Provides the ability to evaluate or manipulate the flow of segments between TCP_Reader and TCP_Writer
via the specific implementation of the AsyncAction method.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xEnableBOOLTRUE: Activates the defined operationFALSE: Aborts/resets the defined operationLConC
Output
xBusyBOOLTRUE: Operation is runningLConC
xErrorBOOLTRUE: Error condition reachedLConC
eErrorIDLConC
Input Const
itfAsyncPropertyitfSegmentPoolInput
itfReaderOutput
itfWriterudiCountUDINT
Properties:
NonBlocking
Methods:
SetInitialValue
ProcessStream
Structure: