Variables (GVL)
- InOut:
Name
Type
Initial
Comment
TECT_FILE_TOKEN
WORD1
1: Reference variable to indicate the zone for which TectLogFile funciton block is running
TECT_FILE_TOKEN_LAST
WORD0
2: Reference variable to indicate the zone for which TectLogFile funciton block has run last
MaxNumberTectTempControlInstances
INT40
3: Maximum number of TectTempControl Instances that can be configured
CurrentTectTempControlInstance
INT0
4: Current number of TectTempControl Instances that are used.This variable needs to be hidden from user access