WARNING_ID (ENUM)

TYPE WARNING_ID(

NO_WARNING

Enumeration of the Warning ID, describes the details of each Warning generated by library function blocks.

Attributes:
qualified_only
InOut:

Name

Initial

Comment

NO_WARNING

0

No warning

DELAYTIME_LONG

-2

Delay time too long compared to temperature gradient TU/TG<0.49 required

RATIO_EXCEEDED

-3

Ratio V1 = TU / TG > maximum value A(iMaxOrd) = A(5), where iMaxOrd = Maximum order of PTn ( n number of PT1(First order elements )connected in series ) model

ADAPTION_CANCELLED

-4

Adaptation cancelled before turning point. Point of inflexion was not reached: use higher step change or use smaller control variable or use SetItg