SolarBackTracking (FUN)
FUNCTION SolarBackTracking : LREAL
This function calculates the optimum tracker position to reduce shadowing by optimizing solar panel position, when position of the sun gets low (early morning + late evening). Axis angle is calculated according to: axis angle for solar tracking in one axis, calculated regardless shadows, distance between rows of Solar Trackers and height of them
Output parameter is the optimum axis angle which avoids shadowing between rows of Solar Trackers. Format: Degrees.
- Dimensional Features
- Example
Shadow effects, early morning, on north to south single axis trackers positioned with the angle calculated regardless shadows, using SolarNSAxisPrimary
Position of the same tracker at the same date, time and location avoiding shadows between rows of trackers by correcting the axis angle with the function block SolarBackTracking
- InOut:
Scope
Name
Type
Initial
Comment
Return
SolarBackTrackingLREALInput
AxisAngleLREAL0
1: Angle of main axis (0°=zenith, anticlockwise). Format: Degrees
PanelLengthREAL1
2: Value that indicates the total length of panels. Format: Meters
DistAxisREAL1
3: Distance between rows of solar trackers. Format: Meters