WARNING_ID (ENUM)
TYPE WARNING_ID : ( // For the function blocks - ModRtuToken, ModRtuRead, ModRtuWrite, ModRtuReadWrite23
NO_WARNING
Enumeration of the Last Warning ID, describes the details of each Warning ID generated by library function blocks.
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_WARNING
16#0
No warning
FUNCTION_INTERRUPTED
16#8010
Read or Write Parameter could not be completed
FUNCTION_ABORTED
16#8011
Function aborted
COM_DIFFERENT_LINE
16#8012
Com interface differs from the actually assigned COM by other blocks on same LineToken variable
NO_CONNECTION_COM_BLOCK
16#8013
No connection to communication block, or error in communication block