ERROR_ID (ENUM)
- TYPE ERROR_ID(
NO_ERROR
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
16#0
No error
INVALID_COM_PORT
16#1
Specified COM port is invalid, check ID or existence of COM port in configuration
MISSING_PARAM_LIST_BUFFER
16#2
Missing reference to parameter list
PARAM_LIST_BUFFER_TOO_SMALL
16#3
Parameter list is not large enough or empty
CFG_READ_FAILED
16#4
Failed to obtain configuration data
UNKNOWN_ERROR
16#FE
unknown error occurred
FATAL_ERROR
16#5FFF
fatal error state