Sm560Send.FB_Init (METH)

METHOD FB_Init : BOOL

FB_Init is always available implicitly and it is used primarily for initialization. The return value is not evaluated. For a specific influence, you can also declare the methods explicitly and provide additional code there with the standard initialization code. You can evaluate the return value.

InOut:

Scope

Name

Type

Comment

Return

FB_Init

BOOL

Input

bInitRetains

BOOL

TRUE: the retain variables are initialized (reset warm / reset cold)

bInCopyCode

BOOL

TRUE: the instance will be copied to the copy code afterward (online change)