Sm560Rec.FB_Exit (METH)

METHOD FB_Exit : BOOL

FB_Exit must be implemented explicitly. If there is an implementation, then the method is called before the controller removes the code of the function block instance (implicit call). The return value is not evaluated.

InOut:

Scope

Name

Type

Comment

Return

FB_Exit

BOOL

Input

bInCopyCode

BOOL

TRUE: the exit method is called in order to leave the instance which will be copied afterwards (online change).