ERROR_ID (ENUM)

TYPE ERROR_ID(

NO_ERROR

Attributes:
qualified_only
InOut:

Name

Initial

Comment

NO_ERROR

0

No error

INVALID_HANDLE

1

Invalid coupler instance handle

DATA_SIZE_INVALID

2

Data size is not the expected one

INVALID_POINTER

3

Invalid pointer found

NO_NETX_CHNL_FOR_SLOTADDR

4

No valid Netx channel on coupler slot

JOB_NOTCREATED

5

No job created

UDISTA_ERR

6

More stack errors possible, further information, if avaiable in output AddErrNo

ASYNC_STATE_BAD

7

Job finished but bad

JOB_RESULT_ERR

8

Job result error, further information in output AddErrNo

STARTJOB_FAULTY

9

Job could not be started

NO_USER_MSG_HDL

10

No user message handle

DATA_SIZE_TOO_BIG

11

Data size is to big (> 84 Bytes)

MSG_TYPE_NOT_SUPPORTED

12

Type (command code) of received message is not supported

RECEIVER_NOT_READY

13

No receiver is ready to receive message

JOB_TIMEOUT

14

Job ends with timeout

JOB_UNKNOWN_ERROR

15

Unknown job error occured

JOB_INVALID_PARAMETER

16

Invalid parametes for job assinged

JOB_PENDING

17

Job is not yet finished

JOB_WRONG_CYCLIC_STATE

18

Job in wrong state

INVALID_INSTANCE

19

Invalid instance handle

REQUEST_FAILED

20

Request has failed, see AddErrNo for details

REQUEST_INVALID_PARAMETERS

21

Request was called with invalid parameters

REQUEST_INTERNAL_ERROR

22

Internal Error occured during execution of request

REQUEST_INVALID_CNF

23

Received invalid confirmation

UNKNOWN_ERROR

100

An unknown error occurred

FATAL_ERROR

16#5FFF

Fatal error of model state machine