ERROR_ID (ENUM)
- TYPE ERROR_ID(
NO_ERROR
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
0
no error
FAILED
1
general error
INVALID_DATA_POINTER
2
invalid pointer to data
DATA_SIZE_LOWER_LIMIT
3
assigned value exceeds lower limit
DATA_SIZE_UPPER_LIMIT
4
assigned value exceeds upper limit
DEVICE_NAME_EMPTY
5
device name string is empty
INVALID_DEVICE_INSTANCE
6
invalid instance of CM579-PNIO assigned at input Device
COM_INDEX_LOWER_LIMIT
7
assigned value of COM index too small
COM_INDEX_UPPER_LIMIT
8
assigned value of COM index too big
DEVICE_IS_NOT_CI504
9
the assigned device name doesn’t belong to a CI504-PNIO device
REQUEST_FAILED
10
request to read or write of serial data was failed
PROTOCOL_ERROR
11
Protocol error, see StatusCode
SUBMODULE_NOT_FOUND
12
specified submodule not found
FATAL_ERROR
16#5FFF
fatal error of model state machine