ERROR_ID (ENUM)
- TYPE ERROR_ID(
NO_ERROR
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
0
No error occurred
FAILED
1
General Error
INVALID_POINTER
3
Invalid pointer
INVALID_HANDLE
4
Invalid handle
INVALID_INSTANCE
5
Invalid instance handle
INVALID_SLAVE_ADDR
6
Slave address has invalid value
INVALID_SLOT_NUMBER
7
Invalid slot number used for DPV1 read/write request
INVALID_INDEX_NUMBER
8
Invalid index number used for DPV1 read/write request
DPV1_DATASIZE_EXCEEDED
20
Maximum size of DPV1 data exceeded
INOUT_DATASIZE_EXCEEDED
21
Maximum size of input/output data exceeded
INOUT_DATALEN_UNDERSIZED
22
More input/output data to be read than expected
REQUEST_FAILED
30
Request has failed, see AddErrorID for details
REQUEST_INVALID_PARAMETERS
31
Request was called with invalid parameters
REQUEST_INTERNAL_ERROR
32
Internal Error occured during execution of request
REQUEST_INVALID_CNF
33
Received invalid confirmation
JOB_ERROR
40
Job ends with an error
JOB_TIMEOUT
41
Job ends with timeout
JOB_UNKNOWN_ERROR
42
Unknown job error occured
JOB_INVALID_PARAMETER
43
Invalid parametes for job assinged
JOB_NOT_CREATED
44
Job was not created
JOB_PENDING
45
Job is not yet finished
JOB_WRONG_CYCLIC_STATE
46
Job in wrong state
UNKNOWN_ERROR
100
An unknown error occurred
FATAL_ERROR
16#5FFF
Fatal error of model state machine