ERROR_ID (ENUM)

TYPE ERROR_ID : ( // Input Validation Errors for all the function blocks

NO_ERROR

Enumeration of the Error ID, describes the details of each Error ID generated by library function blocks.

Attributes:
qualified_only
InOut:

Name

Initial

Comment

NO_ERROR

16#0

No Error

INVALID_INPUT2

16#4020

Invalid value at input 2

WRONG_COMBINATION_INPUT2_3

16#4023

Wrong combination of Inputs 2 and 3

LOW_INPUT3

16#4031

Low value at input 3

INVALID_INPUT3

16#4030

Invalid value at input 3

INVALID_INPUT4

16#4040

Invalid value at input 4

LOW_INPUT4

16#4041

Low value at input 3

LOW_INPUT5

16#4051

Low value at input 5

LOW_INPUT7

16#4071

Low value at input 10

INCOMB_INPUT7

16#4073

Invalid value at input 7

LOW_INPUT10

16#40A1

Invalid value at input 10

INVALID_INPUT11

16#40B0

Invalid value at input 11

WRONG_COMBINATION_INPUT10_11

16#40A3

Wrong combination of Inputs 10 and 11