ERROR_ID (ENUM)
- TYPE ERROR_ID(
JSON_ERR_NO_ERR
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
JSON_ERR_NO_ERR
0
No error.
JSON_ERR_PARSE_ERR
16#3015
Error on parsing given string. Check if JSON string is valid and enough memory is available.
JSON_ERR_STRING_LEN_ERR
16#3017
Error on given string buffer. JSON serialization or string value is longer than string length.
JSON_ERR_KEY_NOT_EXISTING
16#301B
Error on given key. The key does not exist in the JSON object.
JSON_ERR_INDEX_NOT_EXISTING
16#301C
Error on given index. The index does not exist in the JSON array.
JSON_ERR_TYPE_ERR
16#3027
Type mismatch of value at given key in JSON object or at given index in JSON array.
JSON_ERR_MEM_ERR
16#3028
Error on allocating memory on JSON value creation or insertion.
JSON_ERR_INPUT_01_0
16#4010
JsonCreateObject (FUN): Reference parameter JsonObjPtr not initialized.JsonAdd* (FUN): JsonObj not initialized.JsonRemoveEntry (FUN): JsonObj not initialized.JsonSerializeObject (FUN): JsonObj not initialized.JsonGet* (FUN): JsonObj not initialized.JsonParseObjectFromString (FUN): Reference parameter JsonObjPtr not initialized.JsonFreeObject (FUN): JsonObj not initialized.JsonCreateArray (FUN): Reference parameter JsonArrayPtr not initialized.JsonArrayAdd* (FUN): JsonArray not initialized.JsonArrayRemoveEntry (FUN): JsonArray not initialized.JsonSerializeArray (FUN): JsonArray not initialized.JsonArrayGet* (FUN): JsonArray not initialized.JsonParseArrayFromString (FUN): Reference parameter JsonArrayPtr not initialized.JsonFreeArray (FUN): JsonArray not initialized.JSON_ERR_INPUT_01_1
16#4011
Function Input 01 error 1, specific error depends on used function:,
JsonAdd* (FUN): JsonObj does not point to valid JSON object.JsonRemoveEntry (FUN): JsonObj does not point to valid JSON object.JsonSerializeObject (FUN): JsonObj does not point to valid JSON object.JsonGet* (FUN): JsonObj does not point to valid JSON object.JsonFreeObject (FUN): JsonObj does not point to valid JSON object.JsonArrayAdd* (FUN): JsonArray does not point to valid JSON array.JsonArrayRemoveEntry (FUN): JsonArray does not point to valid JSON array.JsonSerializeArray (FUN): JsonArray does not point to valid JSON array.JsonArrayGet* (FUN): JsonArray does not point to valid JSON array.JsonFreeArray (FUN): JsonArray does not point to valid JSON array.JSON_ERR_INPUT_02_0
16#4020
Function Input 02 error 0, specific error depends on used function:,
JsonAdd* (FUN): KeyName not initialized.JsonRemoveEntry (FUN): KeyName not initialized.JsonSerializeObject (FUN): StringBuffer not initialized.JsonGet* (FUN): KeyName not initialized.JsonParseObjectFromString (FUN): JsonString not initialized.JsonSerializeArray (FUN): StringBuffer not initialized.JsonArrayAddReal (FUN): RealValue stored at invalid memory location.JsonArrayAddString (FUN): StringValue not initialized.JsonArrayAddObject (FUN): JsonObjValue not initialized.JsonArrayAddArray (FUN): JsonArrayValue not initialized.JsonParseArrayFromString (FUN): JsonString not initialized.JSON_ERR_INPUT_02_1
16#4021
Function Input 02 error 1, specific error depends on used function:,
JsonArrayAddObject (FUN): JsonObjValue does not point to valid JSON object.JsonArrayAddArray (FUN): JsonArrayValue does not point to valid JSON array.JSON_ERR_INPUT_03_0
16#4030
Function Input 03 error 0, specific error depends on used function:,
JsonAddReal (FUN): RealValue stored at invalid memory location.JsonAddString (FUN): StringValue not initialized.JsonAddObject (FUN): JsonObjValue not initialized.JsonAddArray (FUN): JsonArrayValue not initialized.JsonGetBool (FUN): Reference parameter BoolValue not initialized.JsonGetInt (FUN): Reference parameter IntValue not initialized.JsonGetReal (FUN): Reference parameter RealValue not initialized.JsonGetString (FUN): Reference parameter StringValue not initialized.JsonGetObject (FUN): Reference parameter JsonObjPtr not initialized.JsonGetArray (FUN): Reference parameter JsonArrayPtr not initialized.JsonArrayGetBool (FUN): Reference parameter BoolValue not initialized.JsonArrayGetInt (FUN): Reference parameter IntValue not initialized.JsonArrayGetReal (FUN): Reference parameter RealValue not initialized.JsonArrayGetString (FUN): Reference parameter StringValue not initialized.JsonArrayGetObject (FUN): Reference parameter JsonObjPtr not initialized.JsonArrayGetArray (FUN): Reference parameter JsonArrayPtr not initialized.JSON_ERR_INPUT_03_1
16#4031
Function Input 03 error 1, specific error depends on used function:,
JsonAddObject (FUN): JsonObjValue does not point to valid JSON object.JsonAddArray (FUN): JsonArrayValue does not point to valid JSON array.