General
Here are the function block ETHxOwnIP to get the IPs of PLC’s Ethernet Interfaces and the function block ETHxOwnIPInfo to get information of the IPs of PLC’s Ethernet Interfaces.
GeneralHere are the function block ETHxOwnIP to get the IPs of PLC’s Ethernet Interfaces and the function block ETHxOwnIPInfo to get information of the IPs of PLC’s Ethernet Interfaces.