ERROR_ID (ENUM)

TYPE ERROR_ID(

NO_ERROR

Attributes:
qualified_only
InOut:

Name

Initial

Comment

NO_ERROR

0

No error

ERR_FAILED

1

General error

ERR_PARAMETER

2

Parameter error

ERR_JOB_PARAMETER

3

Job could not be created

ERR_TIMEOUT

5

Timeout error

ERR_ADAPTER

6

Failed to get adapter information, probably invalid interface specified

ERR_FILE

7

Failed to handle a configuration file (open, close or write)

ERR_CONVERT

8

Failed to convert a value

JOB_ERROR

21

Job ends with an error

JOB_TIMEOUT

22

Job ends with timeout

JOB_UNKNOWN_ERROR

23

Unknown job error occured

JOB_INVALID_PARAMETER

24

Invalid parametes for job assinged

JOB_NOT_CREATED

25

Job was not created

JOB_PENDING

26

Job is not yet finished

UNKNOWN_ERROR

100

An unknown error occurred

INVALID_INPUT_ETH

16#4020

Wrong value on input #2 (ETH)

INVALID_INPUT_IPADR

16#4030

Wrong value on input #3 (IP address)

INVALID_INPUT_NETMASK

16#4040

Wrong value on input #4 (Netmask)

INVALID_INPUT_HOSTNAME

16#4021

Wrong value on input #2 (Hostname) DNS POU

INVALID_INPUT_IPADRSERVER

16#4031

Wrong value on input #3 (Ip address of server) DNS POU

INVALID_INPUT_VPNSTATE

16#4041

Wrong value on input #1 (VPN Control)

FATAL_ERROR

16#5FFF

Fatal error state machine