WARNING_ID (ENUM)
TYPE WARNING_ID : ( // For function blocks DrvModbusRead and DrvModbusWrite.
NO_WARNING
Enumeration of the Last Warning ID, describes the details of each Warning ID generated by library function blocks.
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_WARNING
16#0
No warning
FUNCTION_INTERRUPTED
16#7001
Read or Write Parameter could not be completed
FUNCTION_ABORTED
16#7008
Function aborted
COM_DIFFERENT_LINE
16#700B
Com interface differs from others on same LineToken variable
NO_CONNECTION_COM_BLOCK
16#700F
No connection to communication block or error in communication block
READ_PRM_FAILED
16#700D
Fieldbus Read_Parameters was executed with error
WRITE_PRM_FAILED
16#700E
Fieldbus Write_Parameters was executed with error
PING_ECHO_REQ
16#301A
Target Host did not answer the ping echo request before the specified timeout
SPEED_REF_SCALED_VALUE_TOO_LOW
16#7010
Value of rSpeedRefScaled is too low i.e <-32768, scaling is done as per formula rSpeedRefScaled := ( SpeedRef / SpeedRefMax ) * SpeedScaleMax
SPEED_REF_SCALED_VALUE_TOO_HIGH
16#7011
Value of rSpeedRefScaled is too high i.e >32767, scaling is done as per formula rSpeedRefScaled := ( SpeedRef / SpeedRefMax ) * SpeedScaleMax
TORQUE_REF_SCALED_VALUE_TOO_LOW
16#7012
Value of rTorqueRefScaled is too low i.e <-32768, scaling is done as per formula rTorqueRefScaled := ( TorqueRef / TorqueRefMax ) * TorqueScaleMax
TORQUE_REF_SCALED_VALUE_TOO_HIGH
16#7013
Value of rTorqueRefScaled is too high i.e >32767, scaling is done as per formula rTorqueRefScaled := ( TorqueRef / TorqueRefMax ) * TorqueScaleMax
INVALID_INPUT_SPEED_REF
16#7014
Invalid value at input ‘SpeedRef’, Valid range: -20000 .. +20000. Value will be limited to maximum (20000) if SpeedRef > 20000 and the value will be limited to minimum (-20000) if SpeedRef < -20000
INVALID_INPUT_REF_VALUE2
16#7015
Invalid value at input ‘RefValue2’, Valid range: -10000 .. +10000. Value will be limited to maximum (10000) if RefValue2 > 10000 and the value will be limited to minimum (-10000) if RefValue2 < -10000