Errors (GVL)
AC500-specific error definitions
- InOut:
Scope
Name
Type
Initial
Comment
Constant
ERR_OEM_START
RTS_IEC_RESULT16#8000
OEM error range start
ERR_AC500_IN_USE
RTS_IEC_RESULT(ERR_OEM_START + 16#1)
entry already or still in use
ERR_AC500_NULL_REFERENCE
RTS_IEC_RESULT(ERR_OEM_START + 16#2)
NULL reference given, e.g. NULL pointer in function call
ERR_AC500_VALUE_NOTEXPECTED
RTS_IEC_RESULT(ERR_OEM_START + 16#3)
value given is not expected here, e.g. value == 0 but has to be > 0
ERR_AC500_PARAMETER_NOT_FOUND
RTS_IEC_RESULT(ERR_OEM_START + 16#4)
parameter ID given was not found in referenced connector
ERR_AC500_PARAMETER_VALUE_UPPER_LIMIT
RTS_IEC_RESULT(ERR_OEM_START + 16#5)
value of parameter in configuration exceeds upper limit
ERR_AC500_PARAMETER_VALUE_LOWER_LIMIT
RTS_IEC_RESULT(ERR_OEM_START + 16#6)
value of parameter in configuration exceeds lower limit
ERR_AC500_PARAMETER_VALUE_OUT_OF_LIMITS
RTS_IEC_RESULT(ERR_OEM_START + 16#7)
value of parameter in configuration exceeds upper or lower limit
ERR_AC500_PARAMETER_VALUE_NOT_SUPPORTED
RTS_IEC_RESULT(ERR_OEM_START + 16#8)
value of parameter in configuration is not supported
ERR_AC500_CONNECTOR_NOT_FOUND
RTS_IEC_RESULT(ERR_OEM_START + 16#9)
required connector was not found in configuration
ERR_AC500_CONNECTOR_WRONG_TYPE
RTS_IEC_RESULT(ERR_OEM_START + 16#A)
assigned connector has not the expected type
ERR_AC500_NETX_REQ_NEGATIVE_RESP
RTS_IEC_RESULT(ERR_OEM_START + 16#B)
negative response of a netx request received
ERR_AC500_CONFIGURATION_INCOMPATIBLE
RTS_IEC_RESULT(ERR_OEM_START + 16#C)
configuration doesn’t match with IODriver implementation
ERR_AC500_FAILED_TO_REGISTER
RTS_IEC_RESULT(ERR_OEM_START + 16#D)
registration of a handler function etc. wasn’t successful
ERR_AC500_FAILED_TO_UNREGISTER
RTS_IEC_RESULT(ERR_OEM_START + 16#E)
un-registration of a handler function etc. wasn’t successful
ERR_AC500_NOT_REGISTERED
RTS_IEC_RESULT(ERR_OEM_START + 16#F)
a required element was not registered
ERR_AC500_NOT_CONFIGURED
RTS_IEC_RESULT(ERR_OEM_START + 16#10)
a required element was not configured
ERR_AC500_CONFIG_DATA_CORRUPT
RTS_IEC_RESULT(ERR_OEM_START + 16#11)
serious error in configuration data
ERR_AC500_ENTRY_NOT_FOUND
RTS_IEC_RESULT(ERR_OEM_START + 16#12)
an entry was not found
ERR_AC500_ENTRY_FOUND
RTS_IEC_RESULT(ERR_OEM_START + 16#13)
an entry was found
ERR_AC500_OBJECT_CREATE_FAILED
RTS_IEC_RESULT(ERR_OEM_START + 16#14)
an object could not be created
ERR_AC500_INSTANCE_IN_USE
RTS_IEC_RESULT(ERR_OEM_START + 16#15)
instance is still in use
ERR_AC500_ITF_CORRUPT
RTS_IEC_RESULT(ERR_OEM_START + 16#16)
serious error in interface - at least one required reference not set
ERR_AC500_ITF_OUT_OF_OEM_RANGE
RTS_IEC_RESULT(ERR_OEM_START + 16#17)
an interface ID is not inside defined OEM range
ERR_AC500_IO_AREA_NOT_EXISTING
RTS_IEC_RESULT(ERR_OEM_START + 16#18)
Input or Output area doesn’t exist, due to no IO channels configured
ERR_AC500_ABORTED
RTS_IEC_RESULT(ERR_OEM_START + 16#19)
something was aborted
ERR_AC500_FILE_NOT_EXISTING
RTS_IEC_RESULT(ERR_OEM_START + 16#1A)
file doesn’t exists and couldn’t be opened
ERR_AC500_NETX_REQ_UNKNOWN
RTS_IEC_RESULT(ERR_OEM_START + 16#1B)
netx request is not supported
ERR_AC500_NO_PROD_DATA
RTS_IEC_RESULT(ERR_OEM_START + 16#1C)
device has no production data
ERR_AC500_MSG_NO_RESPONSE
RTS_IEC_RESULT(ERR_OEM_START + 16#1D)
no response for a message received
ERR_AC500_MSG_INVALID_CRC
RTS_IEC_RESULT(ERR_OEM_START + 16#1E)
invalid CRC of a received message
ERR_AC500_MSG_INVALID_DATA
RTS_IEC_RESULT(ERR_OEM_START + 16#1F)
data or data structure of a received message is invalid
ERR_AC500_DEVICE_NOT_OPENED
RTS_IEC_RESULT(ERR_OEM_START + 16#20)
device (e.g. com port) was not opened before usage
ERR_AC500_DEVICE_ALREADY_OPENED
RTS_IEC_RESULT(ERR_OEM_START + 16#21)
device (e.g. com port) is already opened
ERR_AC500_CYCLE_TIME_TOO_LOW
RTS_IEC_RESULT(ERR_OEM_START + 16#22)
cycle time is too low for task execution