CommAbbxUsrMsgGet (FUN)
FUNCTION CommAbbxUsrMsgGet : RTS_IEC_HANDLE
open an existing instance for user communication purposes result of this function is a handle which allows use of send/receive functionality
it’s not required to put the obtained handle since it is managed internally in firmware layers
- InOut:
Scope
Name
Type
Comment
Return
CommAbbxUsrMsgGetRTS_IEC_HANDLEInput
psChannelPOINTER TO AC500_NetxBase.tsNetxChannel
channel reference, use AC500_NetxBase.CommNetxGetChannel (NetxBase)