|
This is the web edition of the original ⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements. |
Automation Builder 2.3.x (and newer) has an integrated Safety Verification Tool (SVT) that is installed with the AC500-S software package as a part of the Automation Builder installation.
SVT verifies the AC500-S safety configuration in Automation Builder and generates an SVT checklist that AC500-S users shall use to manually complete the functional safety verification of the Automation Builder project.




DANGER

SVT is mandatory for use with Automation Builder 2.3.x (and newer).
In Automation Builder 2.2.x and earlier versions, there was no need to use SVT due to other procedures used to verify the functional safety integrity of the Automation Builder project.
Use SVT to verify that the safety project in AC500-S Programming Tool matches your safety project in Automation Builder.