SUBPermalink

IEC operator: Subtraction of one variable from another of the types: BYTE, WORD, DWORD, SINT, USINT, INT, UINT, DINT, UDINT, REAL and LREAL.

⮫ “Overview”

A TIME variable may also be subtracted from another TIME variable resulting in third TIME type variable. Note that negative TIME values are undefined.

Example in ST:

‎ var1 := 7-2;‎

Example in FBD:

sub