Configuration of communication parameters in WindowsPermalink

Configuration of communication parameters

To set up communication between the PC and the PLC, e.g., for downloading the compiled program, the communication parameters must be configured.

The IP address of the PC must be in the same class as the IP address of the CPU.

The factory IP address of the CPU is 192.168.0.10.

The IP address of the PC should be 192.168.0.X (avoid X = 10 in order to prevent an address conflict).

The subnet mask should be 255.255.255.0.

Changing of the IP address

  1. Open the Windows Control Panel. Click “Network Status  Network and Sharing Center”.

  2. Select “Change adapter settings”.

    When using existing network with multiple devices, network rules must be observed or a system administrator consulted.

  3. Right-click “Local Area Connection (Ethernet)” and select [Properties].

  4. SE_Local_Area_Connection_Properties

    Double-click “Internet Protocol Version 4 (TCP/IPv4)”.

  5. SE_Internet_Protocol_Version

    Enter the required IP address and subnet mask.