Command 'Run Static Analysis'Permalink

Symbol: sa_icon_runstaticanalysis.png

Function: The command starts the static analysis for the active application and displays the results in the message view.

Call: Menu bar: “Build  Static Analysis”

During the code analysis, CODESYS generates code just like the “Build  Generate Code” command. The results of the analysis are displayed as errors sa_icon_runstaticanalysis.png and warnings sa_icon_warning in the message view (“Build” category). The numbers refer to the corresponding rules as they are defined in the project settings. The syntax for the displayed messages is “SA<rule number:<rule text>”.

See also