'Project' 'Object' 'Convert'Permalink

This command can only be used with POUs. You can convert POUs from the languages ST, FBD and LD, into one of the two languages FBD and LD.

For this the project must be compiled. Choose the language into which you want to convert and give the POU a new name. Remember that the name of the POU may not have already been used. Then press 'OK', and the new POU is added to your POU list.

The type of processing that occurs during conversion corresponds to that which applies to compilation.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

Actions cannot be converted.

proj_obj_konvert (AC500-S PT)

Note the following possibility: A POU which has been created in the FBD-Editor can, using the command 'Extras' 'View' be displayed and edited in the KOP-Editor as well without any conversion.

⮫ “'Extras' 'View'”