Print marginsPermalink

The vertical and horizontal margins that apply when the editor contents are printed, are shown by red dashed lines if the 'Show print range' option in the project options in the dialog 'Workspace' was selected. The properties of the printer that was entered apply, as well as the size of the print layout selected in the 'File' 'Printer Setup' menu. If no printer setup or no print layout is entered, a default configuration is used (Default.DFR and default printer). The horizontal margins are drawn as if the options 'New page for each object' or 'New page for each sub-object' were selected in 'Documentation settings'. The lowest margin is not displayed.

⮫ “'File' 'Printer setup'”

An exact display of the print margins is only possible when a zoom factor of 100% is selected.