Multiple write access on outputPermalink

This function of the 'Project' 'Check' menu searches for memory areas to which a single project gains write access at more than one place. The output then appears as follows:

%QB24 is written to at the following locations:

PLC_PRG (3): %QB24

PLC_PRG.POU1 (8): %QB24

Results are displayed in the message window.