Installation of safety modulesPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

The following rules shall be taken into account for installing safety modules:

  • The installation must be done according to the documentation with appropriate facilities and tools.

  • The installation of the devices may be done only in de-energized condition and carried out by the qualified personnel.

  • The general safety regulations and applicable national safety regulations shall be strictly observed.

  • The electrical installation shall be carried out in accordance with relevant regulations.

  • Take the necessary protective measures against static discharge.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

PLC damage due to wrong enclosures

AC500-S safety modules shall be used in enclosed switchgear cabinets which are suitable for modules with IP 20 degree of protection.

⮫ “Control cabinet assembly (indoor use)”