'Insert' 'Type'Permalink

With this command you will receive a selection of the possible types for a declaration of variables. You also receive the list when you access the input assistant (<F2>).

The types are divided into the following categories:

  • Standard types BOOL, BYTE, etc.

  • Defined types Structures, enumeration types, etc.

  • Standard function blocks for instance declarations

  • Defined function blocks for instance declarations

All standard types of IEC1131-3 are supported.

⮫ “ARRAY”