'Insert' 'Coil' in LDPermalink

kopsymb_spule (AC500-S PT)

Shortcut: <Ctrl>+<L>

You can use this command in the LD editor to insert a coil in parallel to the previous coils.

⮫ “Coil”

If the marked position is a connection between the contacts and the coils, then the new coil will be inserted as the last. If the marked position is a coil, then the new coil will be inserted directly above it.

⮫ “Cursor positions in the LD editors”

⮫ “'Insert' 'Contact' in LD”

The coil is given the text "???" as a default setting. You can click on this text and change it to the desired variable. For this you can also use the input assistant.

⮫ “'Edit' 'Input assistant'”

For the possibility of entering addresses, of linebreaks for variable names and of comments per coil please see the description of the Ladder Options dialog.