'Insert' 'Box with EN in LD'Permalink

kop_symbol_box_en (AC500-S PT)

Use this command to insert a function block, an operator, a function or a program with EN input into a LD network.

The marked position must be the connection between the contacts and the coils (Cursor Position 4) or a coil (Cursor Position 3). The new POU is inserted in parallel to the coils and underneath them; it contains initially the designation "AND". If you wish, you can change this designation to another one. For this you can also use the input assistant.

⮫ “'Edit' 'Input assistant'”