'Extras' 'Negation'Permalink

fupsymb_extras_neg (AC500-S PT)

Shortcut: <Ctrl>+<N>

With this command you can negate the inputs, outputs, jumps, or RETURN instructions. The symbol for the negation is a small circle at a connection.

If an input is selected (Cursor Position 2), then this input will be negated.

⮫ “Cursor positions in FBD”

If an output is selected (Cursor Position 4), then this output will be negated.

If a jump or a return is marked, then the input of this jump or return will be negated.

A negation can be canceled through renewed negation.