Dialog 'Target Settings'Permalink

The dialog 'Target Settings' will open automatically, when a new project is created. It also can be opened by selecting the menu item 'Target Settings' in the register 'Resources' in the Object Organizer.

Choose one of the target configurations offered at Configuration.

If you choose one of the installed configurations it depends on the entries in the target files, which possibilities are left to customize this configuration in the dialogs.

If a configuration is selected, which is provided with the entry "HideSettings" in the corresponding target file, you only can see the name of the configuration. Otherwise you can use the visualization dialog to modify the given configuration.

⮫ “Target settings in category visualization”

Please be aware, that each modification of the predefined target configuration can cause severe changes in performance and behavior of the target!

Press <Default> if you want to reset the target settings to the standard configuration given by the target file.