Declaration partPermalink

All variables to be used only in this POU are declared in the declaration part of the POU. These can include: input variable, output variable , input/output variables, local variables, remanent variables and constants. The declaration syntax is based on the IEC61131-3 standard.

⮫ “Input variable”

⮫ “Output variable”

⮫ “Input and output variables”

⮫ “Local variables”

⮫ “Constants, typed literals”

Regard the possibility of using templates for objects of type 'Global Variables', 'Data types', 'Function', 'Function Block' or 'Program'.

⮫ “'Save as template'”

Regard the possibility of using pragmas to affect the properties of a variable concerning the compilation resp. precompilation process.

⮫ “Pragmas, overview”

An example of a correct declaration of variables in the editor:

editor_dekl (AC500-S PT)