Besides the configuration of the individual visualization elements also the visualization object as a whole can get configured. This is possible concerning the settings for frame, language, grid, background, placeholders etc. as well as the assignment of special hotkey definitions (keyboard usage), which should be valid for exactly one visualization object. These settings are done in the visualization editor via commands of the 'Extras' menu.
Besides that outside of the editor you can do some settings in the Properties dialog of the visualization object, which concern the usage as web visualization or as Master layout.
Regard that in the project options a separate directory can be defined for visualization files.
Image files can be used for the background (static) of a visualization in "bitmap" elements (static or dynamic use).