GeneralPermalink

In a project, the target system can be changed by changing the processor module type or the terminal base type. If possible, the device configuration of fieldbuses and interfaces is retained and transferred to the device configuration of the new module.

Target change options:

  • Between platforms: from V2 platform to V3 platform and vice versa.

  • Between module types: from AC500 (standard) to AC500-eCo and vice versa.

  • A combination of a platform change and a module type change.