ATANPermalink

IEC operator: Returns the arc tangent (inverse function of tangent) of a number.

⮫ “Overview”

IN can be type BYTE, WORD, DWORD, INT, DINT, REAL, SINT, USINT, UINT, UDINT. The result OUT is calculated in radians and must be type REAL.

Example in ST:

‎q:=ATAN(0.5);‎

Example in FBD:

atan