Visualization Element: Text Field Permalink

Symbol:

_visu_img_text_field.png

Category: “Common Controls”

The element can output text statically.

  • The contents of a variable can be part of the text.

  • Show tooltips. The text is managed as static text and can also be defined so that the contents of a variable are also displayed.

  • Display text dynamically. Texts of a text list are displayed dynamically.

  • Used for a text input. For example, a user can input a number or a text literal.