Symbol:

Category: “Alarm Manager”
The element displays alarms in a list. In the element properties, you specify which information is shown. You define the appearance of the element and the variables that control the element behavior.
In online mode, you can sort an alarm table by a specific column – even in the "classic" view. Click into the column header. A small triangle indicates the current sort order (ascending, descending). Clicking the symbol reverses the order.
Sorting inside the column depends on the type of the contained information. The “Priority” column is sorted numerically, and the “Message” and “Class” columns alphabetically. The “Value ” and “Latch ” columns may contain different value types. In this case, sorting is first by type
(blank, BOOL, numeric value, string) and then either numerically or alphabetically depending on
the type.
If an alarm history has been created, then you can programmatically delete it at runtime. The recording starts again from the time of deletion.
For more information, see: ⮫ “Visualizing Alarm Management ”, ⮫ Further information
The “Alarm Table” visualization element cannot be inserted into a visualization in the POU pool.