Dialog: Project Settings: Visualization Profile Permalink

Symbol: _visu_icon.png

Function: Configures the settings of the visualization profile

Call: “Project → Project Settings” menu, “Visualization Profile” category

Requirement: A project is open.

Table 858: Visualization Profile

“Specific Profile”

Profile which CODESYS uses in the project and which determines the visualization elements that are available in the project

The list box contains all previously installed profiles.