Dialog: Add Visualization Permalink

Function: Creates a new object with “Visualization” type

Call: “Project  Add Object  Visualization”; context menu of an application

Requirement: An application is selected in the device tree.

“Name”

Name of the visualization

Example: ‎Visu_A‎

The following settings are displayed only when you add a “Visualization” object to the project for the first time.

“Symbol library”

List of all installed symbol libraries

“Assigned”

_cds_icon_option_activated_copy.png: Symbol library is selected

TIP:

CODESYS manages this setting in the project settings.

“Add”

Creates the new visualization and assigns the selected symbol libraries to the project. These are available in the “Visualization Toolbox” view.