Dialog: Access Rights Permalink

Function: The dialog defines the permissions of user groups for a visualization element.

Call: Click in the “Value” field of the “Access rights” element property of a visualization element.

Requirement: A visualization element is selected in a visualization and the “Properties” view is open.

“User groups”

Groups which were configured in the “Visualization Manager” on the “User Management  Groups” tab

“Operational”

_cds_icon_option_activated_copy.png: The visualization element is available with full functionality.

“Only visible”

_cds_icon_option_activated_copy.png: The visualization element is visible only and does not provide any functionality.

“Invisible”

_cds_icon_option_activated_copy.png: The visualization element is not displayed.

“Group hierarchy is used”

Display whether the option “Use group hierarchy” is activated in the “Visualization Manager” on the “User Management  Settings” tab.

A group which is of a higher hierarchy cannot have fewer permissions for an element than an element of a lower hierarchy.

If no user is logged in, then the permissions apply for the visualization elements that are configured for the user group “None”. If the permissions for a visualization element is restricted, then the group “None” should be granted the lowest permissions.