Designing a backgroundPermalink

You can design the background of your visualization in color or with an image. To do this, use the command “Visualization  Background”.

See also

Configuring an image as a background

In addition, you can use the property “Integrate background” in the dialog “Properties” of a visualization object to specify whether the background image should always be displayed in its entirety or whether it should be truncated.

Requirement: A project with a visualization is open.

  1. Open the visualization and select the command “Visualization  Background”.

  2. Activate the option “Image” and open the input assistant.

  3. Select an image in the dialog “Input Assistant”.

    The image serves as a background image.

See also

Configuring a colored background

Requirement: A project with a visualization is open.

  1. Open the visualization and select the command “Visualization  Background”.

  2. Activate the option “Color”.

  3. Select a style color such as “Element background color” from the selection list.

    The background of the visualization is colored.