Command: Visualization Element Repository Permalink

Symbol: _visu_icon.png

Function: The command opens the “Visualization Element Repository” dialog opens for editing the location and visualization profile.

Call: “Tools” menu

Requirement: No project is open.

Repository to manage the visualization profiles and the visualization element libraries

If you want to use your own control, you have the following options:

  • Integrate the control as an HTML5 control

  • Use the control in a frame

    You can configure and use the frame like a visualization element.