Command: Multiply Visu Element Permalink

Symbol: _visu_icon_multiply_element.png

Function: The command opens the “Multiply Visu Element” dialog, which contains a configuration derived from the template element and the array declaration. You can rearrange the elements here, as well as their quantity and the index access to the array data. When you exit the dialog, a field of similar elements is created from the template element. In the properties of the new elements, array variables are now configured with precise array indexes. These new elements are those in which you have configured an array variable with index access placeholders in the template.

Call: “Visualization” menu; context menu

Requirement: The visualization is active and a configured template element is selected.