Dialog 'Project Settings' - 'SVN Settings'Permalink

Symbol: _svn_icon_repository_browser

Function: The behavior of the integrated SVN version control system is configured in this dialog.

Call: Menu bar: “Project  Project Settings” (“SVN Settings”).

Requirement: A project is open.

Table 964: “Automatic locking and merging”

With these settings, you can overwrite the default settings that were made in the dialog “Tools  Options”, category “SVN Settings”.

“Merge”

Behavior for the commands “Update”, “Merge”, or “Switch”, when both sides (working copy and SVN repository) have changed from the base version.

“Locks”

Behavior such as CODESYS SVN objects when they are changed locally.

“Marker”

Behavior for conflicts

Table 965: “Settings SVN version info”

“Create SVN_VERSION_INFO constants for IEC access”

_cds_icon_option_activated: The object ‎SVN_VERSION_INFO‎ is created and includes global constants or variables for the project metadata.

_cds_icon_option_deactivated: The object ‎SVN_VERSION_INFO‎ is not available.

When you activate the option, the object is created automatically. When you deactivate the option, the object is removed from the project automatically.