Symbol:
Function: The command opens the “Update” dialog. In the dialog, the revision is defined for updating the project.
Call:
-
“Project SVN”
-
“Context menu SVN”
If you select nothing or the base node in the object tree, then the entire project is updated to a revision (“Update project to revision”). If you select one or more objects, then these objects are updated and their sub-objects are updated recursively (“Update to revision”). Optionally, you could define that the sub-objects are not updated.
The behavior of the updating process (for example, merging of conflicts) is similar to the “Update project” and “Update” commands.