Command 'Switch'Permalink

Symbol: _svn_icon_copy

Function: This command opens the “SVN switch” dialog. In this dialog, you specify a URL in the SVN repository to which the current working copy of the project is updated. The command switches a project from a branch or tag to another.

Call: Menu bar: “Project  SVN”.

Requirement: The project is versioned.

Dialog 'SVN switch'

“From”

Current SVN URL of the project

“To”

Input field for the target URL in SVN

  • “HEAD”: The “Select revision” dialog opens.

  • _cds_icon_input_assistent: The “SVN Repository Browser” dialog opens. There you select the target URL in the SVN repository.