Command 'Steal locks'Permalink

Symbol: _svn_icon_lock_steal

Function: This command steal the lock of the object. The “Lock Message” dialog opens for this purpose.

Call: Context menu: “SVN”

Requirement: The versioned object is locked by someone else (overlaid with the _svn_icon_lock_steal symbol).

Dialog 'Lock Message'

“Enter the reason why you lock the object:”

Lock message

Example: ‎a.mayer had to steal the lock because the changes need to be implemented so urgently.‎

“Recent Message”

Shows message in the dialog that have already been used. There you select one in order to use the lock message.

“Recursive”

_cds_icon_option_activated: The lock is stolen by the object and all subordinate child objects.

“OK”

Steals the lock.

When the stolen lock is successful, the object (in the object tree) is overlaid with the _svn_icon_status_locked symbol.