Command 'Show properties'Permalink

Symbol: _svn_icon_properties

Function: This command opens the “SVN Properties” dialog. Here you can edit the properties of the versioned object.

Call: Context menu: “SVN”

Requirement: A versioned, unlocked object is selected.

Dialog 'SVN Properties'

Table 954: “properties for: <object name>”

“Name”

Name of the property

Example: ‎myprop:customer-number‎

Note: SVN has some reserved properties. Example: ‎svn:mime-type‎

“Value”

Example: ‎1234‎

Double-click in the field to edit the value.

“Add”

Opens a dialog to define another property with its value.

“Remove”

Deletes the selected property.

“Show binary properties”

_cds_icon_option_activated: The binary properties are also displayed.

“Reset”

Resets the changes displayed in green.

“OK”

Accepts the changes.